Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which are the modular devices compatible with OF/SD in Smartlink ELEC?

The modular devices compatible with OF/SD auxiliaries in Smartlink ELEC are:
Compatible with iOF+SD24 (A9A26897)
• iC60 circuit breaker
• iID residual current circuit breaker
• iSW & iSW-NA switch

Compatible with OF+SD24 (A9N26899)
• C60 or C120 circuit breaker
• DT40, DT60 circuit breaker
• ITG40 residual current circuit breaker
• C60H-DC circuit breaker