How can we help you today?

What is the part number of the spring mounting clips that attach to the box to install an I-Line trim that was provided between July 1994 and August 1997 and a current I-Line hinged trim?

Issue:
Part umber of the spring mounting clips that attach to the box to install an I-Line trim that was provided between July 1994 and August 1997 and a current  I-Line hinged trim.

Product Line:
I-Line Panelboards

Environment:
Installation

Resolution:
This is a 1/4-20 tinneman fastener and the part number is 23301-02203.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre