Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the internal auxiliary contact for the 2510MCG3?
Issue:
Identify the part number for the internal auxiliary contact for the 2510MCG3?

Product Line:
2510 type M manual starters

Environment:
Products sold and used in the United States

Resolution:
It is a 9999SX11 (NO) or 9999SX12 (NC).

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: