Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between D3 and D voltage code for the low consumption D-Line contactors?
Issue:
Difference between D3 and D low consumption D-Line contactors

Product Line:
IEC Contactors and Starters

Environment:
TeSys™ D Contactors

Resolution:
Both coils are rated the same DC voltage.  D3 incidcates the coil provides integral transient suppression.