Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why Can't I connect to a Quantum high end CPU running FW >= 3.6 using UnityPro <= 7.0 ?
The latest Quantum CPU Firmware version compatible with UnityPro 7.0 is the version 3.53

I can connect UnityPro 7.0 (and lower verions) to a Quantum CPU running firmware 3.6 when the CPU is in NOCONF state, but once it is loaded with an application, the connection becomes impossible.

Due to cyber security enhancements, from Quantum CPU FW version 3.6 it is no more possible to connect UnityPro V7.0 (and lower versions) to such a CPU.
There is no other way but upgrading to a later UnityPro/Control Expert software version
side effect : the latest UnityPro version able to connect to Quantum Safety CPUs being UnityPro 7.0, there is no other way but keeping a UnityPro version 7.0 in a dedicated PC or a VM to be able to connect to this CPU range.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings