Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use Resi9 MP on hollow wall?
Issue :
Installation of an enclosure Resi9 MP in a hollow wall.

Product Line :
Resi9 MP

Cause :
IEC 60670-1 standard constraint

Resolution :
Yes it's possible to use Resi MP on hollow wall, because we have a dedicated version with back part in GWT850 as requested by standard for hollow wall installation.

Note :
To select the right enclosure, please chose the commercial reference starting with MIP21, it contains hollow kit installation.
if you need a spare part for the hollow wall kit please refer to MIP99047.
Instruction Sheet of the hollow wall kit : BBV48374
Video : Resi9 MP - Flush Version Installation

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings