Can Start and Stop be performed with an Analog signal on ATV212 drive?
Issue:
Can I start and stop the ATV212 drive with a 4-20ma analog signal?
Product Line:
ATV212
Environment:
All
Cause:
No Start Stop control signal on VFD
Resolution:
No. The start and stop (forward / reverse) commands should be controlled with digital inputs (+24Vdc only).
Can I start and stop the ATV212 drive with a 4-20ma analog signal?
Product Line:
ATV212
Environment:
All
Cause:
No Start Stop control signal on VFD
Resolution:
No. The start and stop (forward / reverse) commands should be controlled with digital inputs (+24Vdc only).
Released for: Schneider Electric Nigeria