What are the details on VW3A3802 option card?
Issue:
Where can I find more information on the VW3A3802 option card?
Product Line:
ATV340 and ATV900 series drives
Environment:
All
Cause:
Safety function expansion module
Resolution:
The VW3A3802 is an advanced machine safety function expansion module for the ATV340 and ATV900 series. https://www.se.com/ww/en/product/VW3A3802/safety-module-advanced-electronic-card,-apm,-24-v-dc/
This adds Safe Stop 1 (SS1), Safe Limited Speed (SLS), Safe Maximum Speed (SMS) and Safe Brake Control (SBC) to the machine safety functions in the drive.
Hardware Requirements:
• If this module is used with the ATV900 series, a VW3A3800 adaptor is required to provide the specific mounting slot for this module. It cannot be mounted into the standard expansion slots on the drive.
• If this module is used with the ATV340 series size D30 or higher, a VW3A3800 adaptor is required to provide the specific mounting slot for this module. It cannot be mounted into the standard expansion slots on the drive.
• Optionally a VW3M8810 ESM distribution unit can be used to simplify termination of the safety inputs.
Drive Firmware Requirements:
The Safety module requires a specific version of firmware to be active on the drive to be compatible. Earlier or later firmware versions will not operate with the Advanced Safety Module VW3A3802.
For ATV900: FW V2.1 IE81
For ATV340: FW V1.6 IE81
Where can I find more information on the VW3A3802 option card?
Product Line:
ATV340 and ATV900 series drives
Environment:
All
Cause:
Safety function expansion module
Resolution:
The VW3A3802 is an advanced machine safety function expansion module for the ATV340 and ATV900 series. https://www.se.com/ww/en/product/VW3A3802/safety-module-advanced-electronic-card,-apm,-24-v-dc/
This adds Safe Stop 1 (SS1), Safe Limited Speed (SLS), Safe Maximum Speed (SMS) and Safe Brake Control (SBC) to the machine safety functions in the drive.
Hardware Requirements:
• If this module is used with the ATV900 series, a VW3A3800 adaptor is required to provide the specific mounting slot for this module. It cannot be mounted into the standard expansion slots on the drive.
• If this module is used with the ATV340 series size D30 or higher, a VW3A3800 adaptor is required to provide the specific mounting slot for this module. It cannot be mounted into the standard expansion slots on the drive.
• Optionally a VW3M8810 ESM distribution unit can be used to simplify termination of the safety inputs.
Drive Firmware Requirements:
The Safety module requires a specific version of firmware to be active on the drive to be compatible. Earlier or later firmware versions will not operate with the Advanced Safety Module VW3A3802.
For ATV900: FW V2.1 IE81
For ATV340: FW V1.6 IE81
Released for: Schneider Electric Nigeria