How can we help you today?

Is the M171 gasket part number ZZ000306 RoHS compliant?

Yes the ZZ000306 M171 gasket is RoHS compliant see attached RoHS document.

Schneider Electric Nigeria

Attachment(s)
370_M16.05_ RoHS_Eliwell Declaration Form 01-01-2019.pdf [326.41 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings