Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Smartlink SIB - Why Cumulative Registers Drop Off after a Power Cycle ?

Product Line

Smartlink SIB - A9XMZA08

Environment
Standalone product.
Connected with Power Monitoring Expert

Issue
Customers that have some Smartlink connected to Power Monitoring Expert complained that some Smartlink registers dropped to an older value after a power cycle of the product.
image.png

Cause of Issue
This is a known issue related to internal memory for devices that have Firmware lower than v2.4.6
Smartlink with Firmware v2.4.2 or lower are concerned.

Resolution
Download EcoStruxure Power Commission v2.20 (EPC)
Connect your Smartlink SIB directly to your EPC.
Launch the Smartlink FW upgrade to v2.4.6 with EPC.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings