How can we help you today?

Where are the System SD Card and Data SD Card slots on the HMIG3U?

Issue
I would like to find where the SD Card slots are on the HMIG3U, for both the System Card and Data Logging card.

Product Line
Harmony HMIG3U (HMIGTU Family)

Environment
Physical HMI

Resolution

In each of the photos below, the top of the photo is the 'back' of the HMIG3U (where you can see the COM port and Ethernet port labels). The bottom of the photo is where the screen is mounted.
With larger screens, the HMIG3U needs to be detached from the screen to be able to open and access the SD CARD slot flap.
Location

SD

Part numbers are as follows:
Replacement 1GB System SD Card required for the HMI to function: HMIZSD1G
4GB SD Card for additional data logging (optional): HMIZSD4G

Schneider Electric Nigeria