Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION7x50 meter with EN50160 Frequency N,N1,N2 counts reset twice per year

Product Line
_____________________________________________________________
ION7650

Environment
_____________________________________________________________

ION Setup
PME Designer

Issue
_____________________________________________________________
When reviewing logged data for EN50160 Freq N, Freq N1, and Freq invld, the values will reset twice a year, First at the start of a new year then again at the start of some month.

Root Cause
_____________________________________________________________
Reset input to Signal limit Evaluation module 1 is pulsed twice in the same year. Logic in the framework is using double "not".

Solution
_____________________________________________________________
Change the Mode setup register of AND/OR module 11 "PQ Sync Yr Inv".
Default value is NOR, setting should be AND
Setup registers of AND/OR 11 module