Search FAQs
What minimum hardware requirement is needed to install EcoStruxure OPC UA Server Expert V2.0 ?
Issue:
Hardware requirement for EcoStruxure OPC UA Server Expert 2.0
Product Line:
EcoStruxure OPC UA Server Expert
Resolution:
EcoStruxure OPC UA Server Expert V2.0 will run on a PC that meets the following minimum standards:
- Either a 32-bit or a 64-bit platform
- Minimum RAM of 4 Gb
- Multicore \ multiprocessor architectures are recommended, to enable optimal runtime performance.
Released for:Schneider Electric Nigeria
Explore more
Explore more