Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
CE15,SP1 cannot find the floating license after updating from CE15
If you update Control Expert from 15 to 15,SP1 without updating the Floating License Manager on the Floating License Server, Control Expert will fail to find the floating license.

To resolve the issue, update the Floating License Manager to version 2.6.  The setup file for Floating License Manager version 2.6 can be found in the folder named 'FloatingLicenseManager' on the Control Expert 15,SP1 installation dvd.

It is not necessary to return the license before updating to version 2.6.

image.png

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings