How can we help you today?

How to to check the hotfixes details installed related to the EcoStruxure Process Expert software ?

This Knowledge base explains different methods available to find the details of Ecostruxure Process Expert hotfixes that are installed in the machine
Method1:  Native feature of EcoStruxure Process Expert
1. Click the about tab in the Engineering client toolbar
about
2. About page opens
3. User shall be able to see the following tabs in the popups
4. General, System details, Client Details, Hotfix Details (Click on the scroll button to see all the options)
5. Click on Hotfix details to get the detailed information about the hotfixes installed
6. The description will give the hotfix details in brief

HF1


Method2: Windows standard method
1. Open the programs and features from the Control panel
2. Navigate to "view installed updates"
3. User shall see the installed hotfixes under the Ecostruxure Process Expert category.

HF2

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings