Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I detect that I have lost communication to an extension rack on a M580 remote drop?

Issue

Extension rack health on remote drop

Product Line

Modicon M580

Environment

EcoStruxure Control Expert

Resolution

You can detect the health of the extension rack by looking at the Device DDT for the CRA. You will find the IO_HEALTH_RACK_1. Each bit of the word corresponds to the slots in the rack. If you lose communication to the whole rack the value will be zero.

Data Editor

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings