How can we help you today?

What are the new features in OFS Server V3.63?

Issue:

New features in OFS Server V3.63

Product Line:
OFS server


Resolution:
The new features are described below:

-Control Expert V14.1 DFB and Program Units private members access
-Access to DFB instances private members, including nested DFBs , for data dictionary symbol link.
-Access to Program Units private members, including DFB instances, for data dictionary symbol link.
The application data dictionary must be configured accordingly in Control Expert.

-Control Expert EBOOL instances Force status management
When forced, a EBOOL instance good quality is OPC_QUALITY_LOCAL_OVERRIDE (0xD8) instead of     OPC_QUALITY_GOOD (0xC0).

- Windows Server 2019 support
- Silent install support
Open a command line, run silentsetup.exe located on the setup image root and follow the instructions.

Schneider Electric Nigeria