How can we help you today?

Can I use the READ_REMOTE EFB to read data from located or unlocated variables in a Unity Quantum PLC?

Issue:
Using the READ_REMOTE EFB to read data from located or unlocated variables in a Unity Quantum PLC


Product Line:
EcoStruxure Control Expert, Modicon Quantum


Resolution:
Yes. The READ_REMOTE block will read data from a remote Unity Quantum PLC that support the Data Dictionary feature  In the Quantum PLC, Data dictionary must be enabled. You must also de-activating the type verification based on checksum comparison using the CTRL parameter. In the second word of the four word array variable for the CTRL, you must enter a value of 1 to de-activate.

Quantum PLC showing unlocated variables with data.

read_remote_Quantum2.PNG


M580 with READ_REMOTE block receiving the unlocated data from the Quantum
read_remote_Quantum1.PNG

Schneider Electric Nigeria