Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use both Level control and booster control on the ATV630 at the same time?

Issue:

Customer wants to use both Booster and level control at the same time

Product Line:

ATV630

Environment:

All

Cause:

When level control is selected, Booster control is not allowing programming.

Resolution:

The level control and booster control are applications and not functions. So depending on the application selected via the macro APPT some parameter will be locked. For example if you select Pump booster control (APPT=Boost) the parameters of the other application will be locked for example: LCM (Level Control Mode) will be deactivated.

So no it is not possible to use the booster control and the level control at the same time.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings