How can we help you today?

Why BMENUA0100 could not be NTP synchronized by Windows 10 NTP Server ?

When windows is used to be the NTP Server to deliver the time to equipment like BMENUA0100, it could happened that the BMENUA0100 is not updating his time.
One parameter inside the W32time register need to be adjusted and this parameter need to be set at 0 as followed :
BMENUA0100 vs Windows 10 NTP Server.PNG

Schneider Electric Nigeria