How do you assign output contactor command to R2 relay on an ATV630 drive?
Issue:
Wants to set R2 for output contactor command
Product Line:
ATV630
Environment:
All
Cause:
Can not assign R2 to output contactor command
Resolution:
To assign R2 to output contactor cmd, first make sure R2 assignment is Not assigned. Then go to Complete Settings / Generic Functions / Output contactor CMD. Then set Output contactor assign to R2. Then go to Complete settings / Error Warning Handling / Output phase loss, and set Output phase loss assign to "No Error Triggered"
Wants to set R2 for output contactor command
Product Line:
ATV630
Environment:
All
Cause:
Can not assign R2 to output contactor command
Resolution:
To assign R2 to output contactor cmd, first make sure R2 assignment is Not assigned. Then go to Complete Settings / Generic Functions / Output contactor CMD. Then set Output contactor assign to R2. Then go to Complete settings / Error Warning Handling / Output phase loss, and set Output phase loss assign to "No Error Triggered"
Released for: Schneider Electric Nigeria