Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there flange kits available for the ATV320 drives?
Issue:
Customer wants a flange kit for the ATV320 drive.

Product Line:
ATV320

Environment:
All

Cause:
Wants to mount the drive with the heatsink out the back of enclosure.

Resolution:
No.  Flange kits are not available for the ATV320 drive

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings