Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Control Expert 15 returns error 'mfc140u.dll is missing' when starting
Control Expert returns the error 'system error: mfc140u.dll is missing' when trying to start.

This error will occur if the mfc140u.dll file already exists on the PC and it is of a newer version when Control Expert is installed.  The 'mfc140u.dll' file is part of the 'Microsoft Visual C++ 20xx Redistributable ' libraries that gets installed during the Control Expert installation process.  Per Microsoft rules, a software installation is not allowed to overwrite an existing version of a Microsoft '.dll' with an older version.  This rule prevented the
proper installation of the required  'Microsoft Visual C++ 20xx Redistributable ' libraries.

image.png


The specific version 'mfc140u.dll' file is essential for the registration of other '.dll's that are included with Control Expert.  As a result of this, the error could also be accompanied with the following error:

image.png

To resolve the issue,
  • Rename the existing .'mfc140u.dll' file.
  • Uninstall Control Expert.
  • Reboot the PC.
  • Reinstall Control Expert.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings