How can we help you today?

Is there any limitation on the fixing position of auxiliary contact blocks on TeSys Giga contactors ?

Maximum 4 auxiliary contact blocks can be fitted to each contactor. When 2 contactors are mechanically interlocked, maximum 3 auxiliary contact blocks can be installed between two contactors.

Schneider Electric Nigeria