Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wiring diagram for the BMXERT1604T Time stamping module?
Issue:
Wiring diagram for the BMXERT1604T Time stamping module


Product Line:
EcoStruxure Control Expert, M580, M340


Resolution:
The wiring for the BMXERT1604T module is as shown below

Wiring Diagram

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: