Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the firmware version of the ATV630 and ATV930 Drives that offers the ethernet cybersecurity features?

Issue:

ATV630 and ATV930 Drives that offers the cybersecurity features with what firmware version?

Product Line:

ATV630 and ATV900 open and enclosed.

Environment:

All

Cause:

Cyber Security for Ethernet

Resolution:

ATV630 Firmware version v3.3IE34 and above have the Ethernet cybersecurity.

ATV930 Firmware version v3.1IE27 and above have the Ethernet cybersecurity.