Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How are the units setup when reading Modbus address 3204 Motor current?

Issue:

Customer is not getting back what he expects when reading motor current 3204 over Modbus.

Product Line:

Altivar drives

Environment:

All

Cause:

Reading Modbus register 3204

Resolution:

Register 3204, Motor current, reads in tenths. Example 200 = 20.0A.