My Site Energy Consumption is not equal to the sum of usages or zones
If the submeters are not metering 100% of the load, the total energy will be lower than the sum of submeters.
If there are sub-sub meters, make sure you do not double count the load:
Example:
In that case, you should not define usage for Meter 1.

If there are sub-sub meters, make sure you do not double count the load:
Example:
- Main Meter
- Meter 1
- Submeter 1.1
- Submeter 1.2
- Meter 2
- Submeter 2.1
- Submeter 2.2
- Meter 1
In that case, you should not define usage for Meter 1.
Released for: Schneider Electric Nigeria