How can we help you today?

What is the width of NE-I unit ?

Issue:
Customer is confused and wants to know the correct width on NE-I unit as there are two values mentioned in the catalog

Environment:
RM6 characteristics

Resolution:
NE-I width is 572 mm as mentioned in catalog extract below for the functional unit dimensions.

image 1