Issue:
How to link variables from Ecostruxure Control Expert to Ecostruxure Operator Terminal Expert 3.2 SP2?
Product Line:
Ecostruxure Control Expert, Ecostruxure Operator Terminal Expert 3.2 SP2
Resolution:
You need to import the variables using the Symbol Link tool in EOTE, as shown below:
1.- Click on Symbol Link under Variables.
2.-Then click on +Symbol above.
3.-Specify your format file .XVM and click on Import.
4.- Browse your .XVM file and click Open.
It is important that there are caveats:
1.- There's no way to "Update" the Link. They have to be deleted and re-Link if changes are made.
2.-If you delete the Link, you lose all your Variables, Logging and Alarms from that old session.
3.- There is no way to pick and choose a subset of Variables to import - which means EVERYTHING gets imported - this could be 100,000 variables... Then you have to delete the variables you don't want ONE BY ONE.
Released for: Schneider Electric Nigeria


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.