Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of Error 5 - 0220040H shows in Micom P13x relay?
Issue:
Meaning of error 5 - 0220040H shows in Micom P13x relay

Product line:
Micom P13x relays

Resolution:
Error 5 - 0220040H means: Static RAM error

If such error occurs and is shown on the HMI display, no control actions can be carried out.
A new attempt to start up the Px3x can only be initiated by turning the supply voltage off and then on again.

Please check the grounding of the relay in the substation proper or not as per our EMC application manual.
Thank to check whether the error show up when switching a circuit breaker, disconnector, or grounding switch Or in conjunction with a lightning?

Thanks to restart all the alarm in device as mention in the below menu:
P13x Error code.GIF
If you find everything is okay but still issue is not resolved then please report the issue with setting, log files & grounding connection clear pictures with reply of above points to our CCC team to support further.

Schneider Electric Nigeria

Attachment(s)
Px3x_Grounding_Application_Guide_EN_EMC.pdf [548.49 KB]