Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Important setting to know from OPCUA Client ?
It’s important to know the following information when there is problem on the OPCUA protocol between the OPCUA client and the OPCUA Server:
We need to know:
  • Simple architecture of the whole system between OPCUA Client and Server and other Network connection
  • OPCUA Client: which SCADA, what is the OPCUA Stack (From OPC Foundation, Unified automation, …), How it is developped the OPCUA client (C#...)?
  • Subscription setting:
    • LifeTimeCount configured from OPCUA client
    • Publishing Interval configured from OPCUA client
    • Session Timeout configured from OPCUA client
  • Monitored Item Setting
    • Sampling Interval configured from OPCUA client
  • Mast Cycle time of the PLC
Example from UaExpert :
  • Subscription setting:
subscription
  • Monitored Item Setting
Setting Monitoring Item

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: