Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Upgrading Control Expert 15.0 SP1 to version 15.1
Before Control Expert 15.0 SP1 can be updated to version 15.1, the following steps must be performed.
  • Export current projects from the project file format (*.STU) into an archive application file format (*.STA).
  • Save the custom libraries.
  • Save any private ASI catalogs.
  • Uninstall Control Expert 15.0 SP1.
  • Reboot the PC.
  • Install Control Expert 15.1.
  • Reboot the PC.
Note: If the reboot steps are not performed, the installation will have problems.