Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is EVlink Home compliant with TIC ?
Yes, depending on the product commercial reference, see in the catalog description, EVlink Home is compatible with TIC (Linky: only historical mode). The anti tripping module ref EVA1HPC1 (1P+N) or EVA1HPC3 (3P+N) can be used with the references that are not compatible with TIC  to prevent the main incomer circuit breakers from tripping.