The floating license can be activated using the alternate method shown in the following steps, if the PC does not have an Internet connection.
- Open the 'floating License Manager'.
- Click on 'Activate'.
- Click on 'Use another activation method'.
- Read and follow the instructions that appears in order to get the floating license activated.
- Click on Next.
- Enter the Activation ID.
- Select the 'Usage Rights'
- Select the number of seats to be used
- Click on Next.
- Enter a path to save the activation request xml file.
- Click on Next.
- Read the 'How to Continue' instructions.
- Transfer the activation Request file to a PC that has an Internet connection. (Do not shutdown the PC or close the 'Floating License Manager' window.)
- Open a web browser.
- Navigate to the url https://se.com/licensing.
- Click on 'Process License Request File'.
- Browse for the ActivationRequest.xml file that was created earlier.
- Click on 'Submit'.
- Click on 'Download' to save the response file.
- Transfer the response file to a temporary folder on the PC that still has the Floating License Manager window opened.
- Click on the 'Browse' button.
- Browse for the response file.
- Click on 'Next'.
- Upon successful activation, the following window should appear.
- Click on 'Finish'.
Released for: Schneider Electric Nigeria