How can we help you today?

Is it possible to activate two setting groups in MICOM P116 model A and model L? How can we activate them? How can we switch between the two groups?

Issue:
Customer has MICOM P116L and wants to activate two setting groups.

Environment:
MICOM P116 settings

Resolution:
Having two setting groups option is available only in MICOM P116 model A (P116A). MICOM P116 model L (P116L) has only one setting group and can not be upgraded nor modified in order to add the two setting groups option since it has a different hardware from that of model A.

Below extract from the manual shows how to activate the two setting groups option in P116A and how to switch between them.

setting group.PNG