Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerChute Network Shutdown is unable to shut down and start up Nutanix Files VMs via SSH when vCenter is offline if on a different subnet than Nutanix Files VMs
Issue:
PowerChute Network Shutdown is unable to shut down and start up Nutanix Files VMs via SSH when vCenter is offline if vCenter is on a different network subnet than the Nutanix Files VMs

Products:
PowerChute Network Shutdown v4.x

Environment:
PowerChute configured with Nutanix support with VMware as hypervisor
vCenter Server deployed as a VM outside or inside of the Nutanix Cluster
Nutanix Files version 3.8.1.1

Solution:
Deploy PowerChute Network Shutdown on the same subnet as the Nutanix Files VMs or modify the firewall rules on the Nutanix Files VMs to allow SSH connection from PowerChute (not recommended).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings