Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where is Altivar Efficiency Calculator located?
Issue:
How to obtain efficiency on Altivar Drives?

Product Line:
Altivar

Environment:
All

Cause:
NA

Resolution:
The following tool uses KW vs HP for its simulation.
https://altivar-efficiency-calculator.se.app/
It is possible to define the loss in function with the following tool. If the motor losses are known , the calculation could be optimized to better reflect the application/rating.