Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can type K cable be used on our ATV212 drive

Issue:
Wants to use type K cable on the ATV212 drive.

Product Line:
ATV212

Environment:
All

Cause:
N/A

Resolution:
Unfortunately, we did not test this kind of cable with our product.
The main issue with the K cable type is the cross section of the cable strand is AWG30. This section is lower than the IEC version we tested in verification and validation test.
Risk is to break some strand when we tighten to the torque specified.

Test in our labs are done with the following cable:

  • Class 5 IEC60228
  • Class C UL486A

So, we can not guarantee the safety with type K cable.