Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV212 be used at high elevation?

Issue:

Customer wants to use the ATV212 at elevation over the maximum elevation listed in the Manual (1000 meters).

Product Line:

Altivar 212

Environment:

Altitude over 1000 meters

Cause:

High elevation jobsite

Resolution:

The ATV212 products is limited at 1000m without derating.

You can reach 3000m with current derating 1 % per 100m.

The limit is 2000m for Corner grounded system.

We can not be higher because the rated insulation of the product is designed for altitude up to 3000m.