How can we help you today?

How do I create logic to toggle an output on/off using a single input bit in Machine Expert Basic?

Issue:
Toggling an output on/off using a single input bit in EcoStruxure Machine Expert Basic


Product Line:
EcoStruxure Machine Expert Basic



Resolution:
Below is a sample logic to turn on and off  the TOGGLE_COIL output using a the PUSHBUTTON bit
image

Schneider Electric Nigeria