Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is ramp switching set up on the ATV900 series Process drive?

Issue:

ATV900 ramp switching set up.

Product Line:

Altivar 930 and 950

Environment:

All

Cause:

Dual ramp rates

Resolution:

Under the Main menu, select Complete settings menu.

Select the Generic functions menu and then Ramp switching

There are 2 ways of doing ramp switching from the typical ACC/DEC settings:

Using frequency threshold

Ramp 2 thd (FRT) assigns an output frequency above which the AC2/DE2 apply. Note that ACC/DEC apply when below the frequency threshold.

Using a logic input to switch ramp

Ramp Switch Assign (RPS) assigns a logic input to activate the second ramp, AC2/DE2.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)