Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Requesting the Altivar drive motor overload trip curve.

Issue:

Requesting the trip curve for the motor overload protection feature of the Altivar drives.

Product Line:

ATV12 ATV212 ATV320 ATV340 ATV600 ATV900

Environment:

All models

Cause:

Estimating trip time

Resolution:

All of the Altivar drives provide motor overload protection based on standard IEC947-4 and therefore use the same trip curves. Please see the attached file.

Schneider Electric Nigeria

Attachment(s)
Altivar thermal protection curve.pdf [658.13 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings