{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can you use a USB C Cable with the TCSMCNAM3M002P and SoMove Software?

Issue:

Will a USB Type-C cable work with the TCSMCNAM3M002P when connecting to an AC Drive with SoMove Software?

Product Line:

Altistart Altivar and Altivar Process Drive

Cause:

USB Type-C with SoMove Software

Resolution:

Tested using using a Female to Female USB Adapter to connect a USB Cable to the TCSMCNAM3M002P Cable, you do get a Com Port Assignment; however, using the same adapter and a cable that is USB to USB C and connecting USB C to laptop, you do not get a Com Port Assignment.

This testing indicates that you can NOT use USB type-C with SoMove Software.

Schneider Electric Nigeria

Can you use a USB C Cable with the TCSMCNAM3M002P and SoMove Software?

Issue:

Will a USB Type-C cable work with the TCSMCNAM3M002P when connecting to an AC Drive with SoMove Software?

 

Product Line:

Altistart Altivar and Altivar Process Drive 

 

Cause

USB Type-C with SoMove Software

 

Resolution:

Tested using using a Female to Female USB Adapter to connect a USB Cable to the TCSMCNAM3M002P Cable, you do get a Com Port Assignment; however, using the same adapter and a cable that is USB to USB C and connecting USB C to laptop, you do not get a Com Port Assignment.

This testing indicates that you can NOT use USB type-C with SoMove Software.

 

Schneider Electric Nigeria
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
move-arrow-top