Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have the expected time difference between the operation of the early make N/O contact on a ZBE201 and the standard N/O Contact on the ZBE101?

Actually, the ZBE*** contact blocks are slow break action that means they are dependent of the head fitted with.

For example, if the customer is using a standard pushbutton, as a ZB4BA*, the speed of actuation of the contact block is directly linked to the speed actuation of the head.

At the opposite, if the customer is using an e-stop, which is a trigger action product like a snap action actuator, the contact block will be actually like that, i.e. closed to a simultaneous actuating.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: