How can we help you today?

What are the NTP restrictions on BMENUA0100 firmware version 2.01?

NTP protocol on BMENUA0100 won’t be available to be configured in the “forward services” in the webpage
BMENUA0100 used as a NTP server will restrict its answers only to a NTP client on its own subnet
BMENUA0100 used as NTP client should only be used on the same subnet as the NTP server BMENUA0100 version 2.01
Environment
Windows, EADM

Schneider Electric Nigeria