What are all the models of HMI that can be programmed with EcoStruxure Operator Terminal Expert v3.3?
What are all the models of HMI that can be programmed with EcoStruxure Operator Terminal Expert v3.3?
Product Line
EcoStuxure Operator Terminal Expert
Environment
HMI Configuration
Resolution
The following file shows a list of all the supported HMI families and models:
"EcoStruxure Operator Terminal Expert v3.3 Supported HMI List.xlsx"
Asterisks [ * ] represent sets of letters indicating iPC variants (RAM, OS, slots, etc).
NOTE:
HMIGTU Open Box specific models HMIG5U and HMIG5U2 (Windows Embedded Standard 7) are not supported in EcoStruxure Operator Terminal Expert. Only the HMIG5U22 (Windows 10 IoT Enterprise LTSC 2019) is supported in EcoStruxure Operator Terminal Expert.
Supported resolutions for iPCs / PCs:
320x240 (QVGA)
640x480 (VGA)
800x480 (WVGA)
800x600 (SVGA)
1024x768 (XGA)
1280x800 (WXGA)
1280x1024 (SXGA)
1366x768 (FWXGA)
1440x900 (WXGA+)
1600x900 (WXGA++)
1920x1080 (FHD)
1920x1200 (WUXGA)
3840x2160 (UHD/4K)
HMI Series Support Changes between EcoStruxure Operator Terminal Expert v3.1 and v3.1 SP1+:
HMIGTO series is no longer supported in EcoStruxure Operator Terminal Expert v3.1 SP1 and higher
As of v3.1 SP1 and higher, Windows-based iPCs are consolidated into the "iPC or PC/AT" category in the
Released for: Schneider Electric Nigeria