Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
XB4 - pilot light , viewing angle > 85°?

The pilot light is visible from 0° to 90° (-90° to +90° by symmetry) but of course with less luminance

To sum up : 60% @ 60° and 40% @ 90°.