Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
E0D00154: internal error exception from Logic Editor
The program can be opened, however when an attempt to make a change in the program the logic editor crashes.
internal error exception

The ucmerr.log is showing an error on usage of msxml4.dll
HRESULT hr=m_pXMLDescriptor.CreateInstance(xml::CLSID_DOMDocument40);
  • This Dll is provide by Windows and should be registered.
Solution:
  • Open Command prompt.
  • Type C:\Windows\SysWOW64>regsvr32.exe msxml4.dll, press enter.
regsvr32
msxml4

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings