There are a number of features of ISaGRAF 3.55 that are not fully supported in SCADAPack Workbench. Some of these are identified in the Workbench CAM3 help and the user will need to modify the ISaGRAF 3.55 project before trying to import it into Workbench.
If the Workbench conversion still fails, one message that could come up is:
"Unsupported feature message true/ message false values: Remove unsupported values from an earlier work bench version"
ISaGRAF 3.55 supported a feature that allowed Boolean variables to have custom terms to identify their state (ex: ON/OFF, OPEN/CLOSED, etc...) instead of only using True or False to identify the state. This is no longer supported in SCADAPack Workbench.To correct the issue, in ISaGRAF 3.55, search through the global and local Boolean variables in the dictionary and delete all names associated with the TRUE/FALSE messages. Please note that a space in the highlighted fields will still count as a message and also needs to be removed before you can import the ISaGRAF 3.55 project into SCADAPack Workbench
Released for: Schneider Electric Nigeria